Search
Languages

Typhoon Doksuri Impact – Bourns (Xiamen) Limited

Riverside, Calif., July 27, 2023

Dear Valued Customers of Bourns,

The government of the People’s Republic of China has mandated that all production must be suspended starting at 3:00 PM on July 26, 2023 in the Xiamen region due to the threat of Typhoon Doksuri. Accordingly, the Bourns manufacturing facility, Bourns (Xiamen) Limited, will be closed July 27 and 28, 2023. Production is expected to resume as soon as it is determined that it is safe for employees to return to work.

Bourns customer service will be directly contacting affected customers regarding pending shipments.

Sincerely,
BOURNS, INC.

James Harrington
Senior Vice President, Worldwide Sales

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf