Search
Languages

Bourns Announces New Sealed Absolute Rotary Encoder Series

Model PAC18R Series Features a Shaft Sealing for an Enhanced Ingress Protection Level and a Precise Rotational Feel

RIVERSIDE, Calif., February 23, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the Model PAC18R Series Sealed Absolute Rotary Encoder. Featuring an IP64 shaft seal rating that delivers an enhanced IP (Ingress Protection) level and a superior rotational feel, the Bourns® Model PAC18R Series provides high quality performance for use in an expanded range of applications where a sealed menu select absolute encoder is required. These applications include professional audio and lighting applications, low/medium risk medical** and diagnostic equipment, and industrial automation controls.

This low profile absolute encoder family has a 30,000 rotational cycle rating and an extended -35 °C to +70 °C operating temperature range. The Model PAC18R Series also offers other advantages such as high contact and insulation resistance values from the device's insulated plastic shaft and bushing as well as a haptic detent feedback option.

The Bourns® Model PAC18R Series is RoHS compliant*** and is available now. For detailed product information, please visit: www.bourns.com/products/encoders/contacting-encoders 

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf