Search
Languages

Bourns Introduces MEMS Environmental Sensor Designed for Ultra-Low Pressure Sensing in a Digital World

RIVERSIDE, Calif., February 25, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new environmental pressure sensor model that provides high accuracy, 3.3 V and ultra-low pressure range capabilities. Bourns® Model BPS125 pressure sensors are based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology and deliver precision performance in a miniature package size. Designed for space-constrained, 3.3 V digital systems that demand extremely sensitive and accurate readings, Bourns® Model BPS125 is capable of measuring pressure in the 250 to 500 Pa range producing an amplified, calibrated pressure reading that can be acquired from the digital interface.

The fully calibrated and compensated digital output offered in Bourns' new model aids in reducing processor workloads and removes the need for A/D conversion while providing long-term stability for reliable repeatability. The combination of features provided by Model BPS125 sensors also helps to improve the performance and efficiency of end applications making them ideal solutions for a range of industrial, consumer and medium/low-risk medical† designs including portable oxygen generators, nebulizers, CPAP equipment, diagnostic spirometers and gas chromatography equipment.

Bourns® Model BPS125 is highly sensitive and stable featuring a Total Error Band (TEB) of 1.5 % FS over a temperature range of 0 °C to +60 °C (Six-Sigma process), and a lifetime drift of 0.5 % FS. The Model BPS125 features I2C digital output, and is offered in 250 and 500 Pa calibrations that assist in minimizing system calibration requirements and help support system uptime. Easily integrated, these new SMT board mount pressure sensors also help to reduce development time.

Bourns has earned its reputation for excellent quality and superior technical support that is backed by the company's global supply chain. Model BPS125 ultra-low pressure sensors are available now and are RoHS compliant*. Bourns also offers customized port configuration and calibration. For more detailed product information, please see: www.bourns.com/docs/product-datasheets/bps125.pdf

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf