Search
Languages

Bourns Announces Flyback Power Transformer Offering Enhanced DC/DC Power Conversion Efficiency in Isolated Mode

RIVERSIDE, Calif., November 21, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced an addition to the company's flyback power transformer line. Designed to support IEEE 802.3 af-compliant, integrated Power-over-Ethernet (PoE) Powered Device (PD) and Pulse Width Modulation (PWM) controller applications, Bourns® Model SM13117EL provides DC/DC power conversion in isolated mode.

The SM13117EL flyback transformer features 13 watts of output power, 36 - 72 VDC/ 250 kHz input, 12 VDC/1.08 amp output and 1.5k Vrms withstanding voltage. This low profile, small form factor PoE flyback transformer also offers an extended -40 to +125 °C operating temperature range, low leakage inductance and excellent EMI performance. Ensuring safe operation, the electrical insulation of the transformer complies with the UL 1446 Class B (130 °C) Insulation System. The transformer bobbin carries the UL 94 V-0 flammability rating.

The features of Bourns' latest flyback power transformer make it an excellent power conversion solution for a broad range of PoE-powered devices including VoIP phones, WLAN access points and network cameras as well as with integrated PoE PD interface and PWM controllers offered by several leading IC manufacturers.

Bourns® Model SM13117EL flyback power transformer is available now and is RoHS compliant*. For more detailed information, please refer to the datasheet: www.bourns.com/docs/product-datasheets/sm13117el.pdf

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf