Search
Languages

Bourns Introduces its Smallest Miniature Resettable Thermal Cutoff (TCO) Devices

RIVERSIDE, Calif., October 16, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced the company's smallest miniature resettable Thermal Cutoff (TCO) devices designed for overtemperature and overcurrent protection of lithium polymer and prismatic cells. The Bourns® Model CB Series is the company's next generation of axial leaded TCO devices that control abnormal, excessive current virtually instantaneously, up to rated limits. This latest series is more than 26 percent smaller than Bourns' successful NR Series, yet has the same current carrying capability. The devices' low-profile 0.8 mm height and body width of 2.5 mm makes this series ideal for smaller batteries in smartphones and portable electronics, yet their high current carrying capability also makes them optimal for next-generation notebook and tablet PC battery cells.

Offering resistance levels as low as 2.2 milliohms, the Bourns® Model CB Series has current capabilities from 6 A up to 11 A at 60 °C as well as a welding projection option. These new miniature resettable TCO devices are available in four trip temperature options of 72 °C, 77 °C, 82 °C and 85 °C with a ±5 °C tolerance. The temperature options can be further narrowed upon request. In addition, the construction of the CB Series uses a high corrosion resistant bimetal mechanism to withstand most humid environments.

Available now, Bourns® Model CB devices are RoHS compliant* and halogen free** with UL agency recognition. For more detailed product information, please see www.bourns.com/products/mini-breakers/product/CB.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

***Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf