Search
Languages

Bourns Acquires Circuit Protection Component Company, KEKO-Varicon d.o.o. Žužemberk

RIVERSIDE, Calif., July 16, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that a member of the Bourns group of companies has acquired all shares of KEKO-Varicon d.o.o. Žužambrek (KEKO-Varicon) from its three shareholders, consisting of two members of the MSIN Group and one minority shareholder. KEKO-Varicon is a leading manufacturer of overvoltage protection products that include varistor and EMI suppression products. Financial terms of the transaction were not disclosed.

Along with adding breadth and depth to Bourns' industry-leading overvoltage and overcurrent protection portfolio, KEKO-Varicon brings a strong employee base, superior overvoltage protection technologies, expanded R&D, and production facility assets as part of the acquisition. Bourns' existing circuit protection portfolio includes gas discharge tubes (GDTs), metal oxide varistors (MOVs), thyristor surge protectors, transient voltage suppressor (TVS) diodes and arrays, Power TVS diodes, Polymer PTC resettable fuses, TBU® High-Speed Protectors (HSPs), mini-breaker thermal cutoff (TCO) devices, and ESD suppressors.

"The acquisition allows Bourns to gain a significant strategic advantage in the range of protection solutions we can offer our customers, particularly in addressing the strict requirements of the automotive industry," said Erik Meijer, President and COO of Bourns, Inc. "Acquiring KEKO-Varicon further reinforces Bourns' ability to meet both complex technology and on-time delivery needs with an even stronger global organization to deliver the highest quality circuit protection devices."

About KEKO-Varicon d.o.o
KEKO-Varicon is one of the world's top manufacturers of overvoltage protective and EMI suppression components. The company's products have been designed into a broad variety of low voltage board level (LVBL), telecommunication, automotive electronics, AC-line, TVSS and high-energy industrial equipment applications. The combination of extensive technical knowledge and advanced equipment enables KEKO-Varicon to produce at almost 0 PPM quality levels. The company‘s headquarters and production facilities are located in Slovenia, EU. Additional company and product information is available at www.keko-varicon.si.

About MSIN Group
MSIN d.o.o. is a Slovenian investment firm with a diverse portfolio of companies. MSIN d.o.o.'s primary focus is to recognize investment opportunities and transform them into successful long-term projects by utilizing its management method, motivated employees and clearly set objectives.

Bourns®, TBU® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

*Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com