Search
Languages

Bourns Introduces Line of Environmental Sensors based on MEMS Technology

RIVERSIDE, Calif., October 29, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new line of environmental sensors based on Micro-Electro-Mechanical Systems (MEMS) technology. The initial products offered in the Bourns Precision Sensor (BPS) line are three pressure sensor model families and one humidity sensor model family. Designed for the advanced sensor needs in Industrial Automation, Energy, Building & Home Control, low/medium-risk Medical* and Mil/Aero applications, the BPS line has been designed to provide high sensitivity/accuracy, long-term reliability, high temperature capability and harsh media compatibility.

Bourns' new sensors feature state-of-the-art technologies that provide the ability to operate in conditions that typically cause many sensors to fail. The BPS110 and BPS120 pressure sensor models deliver extremely accurate ultra-low pressure sensing capabilities for sensitive applications. The BPS110/120 families offer fully calibrated and compensated output for more efficient processes as well as long-term stability for reliable repeatability.

The Model BPS130 pressure sensor line features harsh media compatibility and high temperature operation with high accuracy. This sensor family offers particularly stable performance over the product's lifespan, and the ability to work with a wide range of pressures. Bourns also offers port configuration and calibration customization for all three BPS pressure model families.

The Model BPS230 family offers precision relative humidity sensing in a small (2.0 x 2.0 x 0.75 mm) surface mount package. Bourns' new line of humidity sensors features low current consumption for battery supported applications and low voltage operation compatibility with high reliability over the life of the sensor.

All four Model BPS110, BPS120, BPS130 and BPS230 environmental sensor families are available now. For more detailed product information, please go to: www.bourns.com/products/sensors/environmental-sensors.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

* Bourns® products have not been designed for and are not intended for use in “lifesaving,” “life-critical” or “life-sustaining” applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf