Leave a message
MENU
Search
Languages

Bourns' New 24 mm Potentiometer Capable of Up to 1 Million Shaft Revolutions

RIVERSIDE, Calif., February 5, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released a new 24 mm potentiometer designed for use in light industrial applications such as test and measurement, communications, clean energy and select medical and diagnostic equipment. Supporting the long cycle life and high reliability needed for these applications, the Bourns® Model PDF241 potentiometer features various flatted and slotted shaft lengths and a long-life carbon element that is capable of up to 1 million shaft revolutions.

The latest potentiometer from Bourns has a 0.5 watt power rating and IP40 dust seal rating. It also features an extended temperature (-10 °C to +85 °C) operating range, anti-rotation pin and metal shaft, and is available in a variety of standard resistance values and audio or linear tapers. Available in a bushing mount configuration with standard solder lugs, the new long-life Bourns® potentiometer offers a highly-versatile panel mount solution that delivers excellent reliability and durability.

With sample and production quantities available now, Model PDF241 is also RoHS compliant*. As a pricing reference, Bourns® Model PDF241 potentiometer is priced at $3.89 in quantities of 1,000 pieces. For additional information, please visit: www.bourns.com/products/potentiometers/commercial-panel-controls.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a