MENU
Search
Languages

Bourns Releases New High-Speed CANbus Protectors for Automotive and Industrial Applications

RIVERSIDE, Calif., October 31, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released the company's new high-speed AEC-Q101-qualified Controller Area Network (CAN) protector. Bourns designed its latest surge protection device to protect against damage from transient voltage events such as electrostatic discharge (ESD), interruption of inductive loads or lightning strikes. Ensuring reliable high-speed communications transmission in harsh environments helps systems developers improve reliability in a broad range of automotive and industrial applications that include control networks, Smart Distribution Systems (SDS), DeviceNet™ and factory and process automation systems.

The Bourns® Model CDSOT23-T24CAN-Q (Transient Voltage Suppression) Diode Array features a dual bidirectional TVS for protecting both lines of a single CAN interface. It offers a minimum breakdown voltage of 26.2 V making it an optimal choice for transceivers with internal circuitry to protect against 24 V power supply miswiring. Meeting important international standards, Bourns' new high-speed CANbus protectors provide ±30 kV contact discharge ESD protection per IEC 61000-4-2 and 500 V surge protection per IEC 61000-4-5 (Level 1). It comes in a SOT-23 package, and its compact size eases layout in space-constrained PCB designs while ensuring compliance with stringent EMI requirements.

The Bourns® Model CDSOT23-T24CAN-Q TVS Diode is available now and is RoHS compliant*. As a pricing reference, the Model CDSOT23-T24CAN-Q is priced at $0.11 each for 12,000 pieces. For more information, please go to: www.bourns.com/products/diodes/diode-arrays.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

DeviceNet™ is a trademark of ODVA

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf