MENU
Search
Languages

Strategic acquisition further expands and strengthens Bourns’ leading line of circuit protection GDT solutions

Riverside, Calif., December 4, 2012 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has completed the integration of its acquisition of assets from Jensen Devices AB. This integration included incorporating the acquired Jensen Devices AB products into Bourns' gas discharge tube (GDT) product line, which are available for purchase now, and the transfer of manufacturing from Jensen's factory in Solluntuna, Sweden to Bourns' ISO certified manufacturing facility in Heredia, Costa Rica. The SA2 series of high voltage GDTs are used as overvoltage protectors and the Sparctube® ST series of switching GDTs are utilized in ignition circuits for automotive HID headlights. These GDT products further enhance Bourns' superior technical capabilities, and strengthen the company's circuit protection leadership in several industries including automotive, industrial and telecommunications.

"The successful integration of Jensen Devices products allows Bourns to make a strategic entry into the automotive Xenon headlamp market, which is projected for continued growth through 2016 and beyond," said Dr. Erik Meijer, President of Bourns Electronics. "These products not only strengthen and expand Bourns' GDT line, but benefit our customers by giving them additional product options and design flexibility."

Bourns® Sparctube® ST series of GDTs feature breakdown voltages between 350 V and 1000 V, including the most utilized versions of 800 V and 840 V, which are ideally suited for automotive HID Xenon headlight applications. Characterized by long-term reliability and high temperature performance, the Sparctube® ST series is designed specifically for voltage controlled switching of capacitive discharge circuits where high energy, low loss and a fast rate of switching are required.

The Bourns® SA2 series of high voltage GDTs are designed for high isolation applications such as in street lighting, medical devices, air conditioning units, power supply devices, projectors and welders. The series features high insulation resistance over a wide temperature range and is offered with DC breakdowns from 2.4 kV to 7.2 kV. Other customized voltages are available upon request.

With strategic acquisitions and through the company's internal product development, Bourns has more than 35 years of experience developing GDTs for the circuit protection market. The company is committed to providing the industry's most complete line of circuit protection solutions. Bourns has made 10 acquisitions in the preceding 12 years, including Joslyn Electronics' communication protection products business, Texas Instruments' solid state Telecom protection business, Fultec's Transient Blocking Unit technology and the Protection Product businesses of Corning Cable Systems and Emerson Network Power.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a