Search
Languages

Bourns Introduces Two New Industrial-Grade Panel Control Models

Riverside, Calif., August 23, 2011 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced two new industrial-grade panel control models that include a push-pull switch and rotary switch. Designated the Bourns® Model 54, the new ½-inch panel control is an extension of Bourns® Model 51/53 Series with an added double-pole, double-throw (DPDT) push-pull switch module. The Bourns® Model 56 is a new ½” panel control and is also an extension of the Bourns® Model 51/53 Series with an added single-pole, double-throw (SPDT) rotary switch module. Both new products are high-performance alternatives to readily available consumer-grade potentiometers with push-pull and rotary switches. Developed to match the requirements of a broad range of industrial, medical and aerospace/avionics applications, Bourns’ new panel control models are particularly well-suited for use in test and measurement and communications equipment. Bourns® Model 54 is also an optimal solution for medical diagnostic and professional audio equipment, while the Bourns® Model 56 is designed for use in avionics controls and medical laboratory equipment.

The new models measure 12.5 mm and feature metal bushings and shafts, splash seals and a wide range of linear and audio resistance tapers. Rotational life for both models is 50k cycles with contact resistance at 100 mΩ for Model 54 and 30 mΩ for Model 56. Both models are RoHS compliant.*

"Bourns’ new industrial grade panel controls are significant because they provide the flexibility of a panel control plus push-pull switch or rotary switch in one compact component. In addition, the splash seal provides protection from moisture ingression in a wide variety of applications,” said Chuck Manzano, Product Specialist for Bourns, Inc. “The new panel controls provide designers with high-performance alternatives to consumer-grade potentiometers, providing end customers with enhanced reliability and improved performance as required by industrial, medical and avionics applications.”

Pricing and Availability
Samples and production quantities are now available through Bourns authorized e-Commerce distributors. As a pricing reference, Bourns® Model 54 is priced at $6.95 in 1,000 pc quantities and Model 56 is priced at $5.84 in 1,000 pc quantities through authorized distributors. Data sheets with complete specifications are available on Bourns website at www.bourns.com under Industrial Panel Controls.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com