MENU
Search
Languages

Bourns Announces Industry’s First ECL Designed to Tolerate AC Mains Power Contact without Damage

Riverside, Calif., February 1, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its latest series of TBU® (Transient Blocking Unit) circuit protection devices designed for high speed protection of communications ports. The new devices are the industry’s first electronic current limiters (ECLs) designed to tolerate AC mains power contact without circuit damage. Designated the Bourns® TBU® DT-Series, the new circuit protection device family provides superior protection against faults caused by short circuits, AC power cross, induction and lightning surges. The TBU® DT-Series are very fast-reacting protectors that do not alter the signal performance of high speed communication ports unlike high capacitance protectors. The new Bourns® TBU® devices are an optimal solution for Ethernet ports used in outdoor applications such as security systems, PV panels and service kiosks.

“The TBU DT-Series represents a whole new level of circuit protection for sensitive Ethernet ports,” said Ian Doyle, product line manager of semiconductor products at Bourns, Inc. “Ethernet interfaces today are used almost everywhere and are exposed to ever more serious threats Superior protection without compromising performance is now possible for high speed Ethernet ports thanks to the fast-acting capabilities of these devices.”

The new devices provide an integrated solution that minimizes design and manufacturing costs for design engineers that translates into faster time-to-market. In addition, they enable a lower component count that meets OEM demands for smaller circuit boards in space-constrained designs. Protecting against a wide range of hazardous threats, the Bourns® TBU® DT-Series also helps customers eliminate expensive maintenance, repair and system downtime costs.

The Bourns® TBU® DT-Series features eight models and offers continuous AC voltage ratings up to 425 Vrms and nominal trigger currents ranging from 150 mA to 750 mA. The new device family comes in a surface mount DFN package and is lead free and RoHS* compliant. Product samples are available now through Bourns’ distribution partners. As pricing examples, Bourns® TBU-DT-065 and TBU-DT-085-XXX-WH are priced at $.69 each in 15K quantities.

About Bourns® TBU® Technology
The Bourns® TBU® High Speed Protector is an innovative approach to electronics circuit protection. It is designed to block a transient through a current disconnecting mechanism. Rather than a complex interstage coordination between two shunting components, the TBU® device protects systems from both overvoltage and overcurrent surges. The TBU® device provides protection within nanoseconds, essentially eliminating latency common in the circuit protection design, limiting let-through energy. Bourns® TBU® devices have virtually no capacitance or inductance, and therefore can be used in high speed and high bandwidth applications. The TBU® DT-Series features unidirectional operation which is inherently resettable.

*RoHS Directive 2002/95/EC January 27, 2003 including Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf