Leave a message
MENU
Search
Languages

Bourns Launches New SinglFuse™ Line of Thin Film Chip Fuses

RIVERSIDE, Calif, September 23, 2008 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its SinglFuse™ SF Series of thin film chip fuses. This new line provides highly reliable overcurrent protection in three surface mountable footprint sizes. Each product size features two series to cover the fusing types of fast-acting and slow-blow. The new SinglFuse series expands Bourns’ comprehensive circuit protection portfolio with a line of thin film chip fuses for use in applications such as LCD monitors, digital cameras, cell phones, industrial controllers and rechargeable battery packs.

Bourns’ SinglFuse products protect against a wide range of overcurrent events and feature current ratings from as low as 500 m amps up to 7 amps. The thin film design of Bourns’ new SinglFuse products ensures high precision for specific fusing characteristics. Single-use thin film chip fuses are specifically designed for applications which require one-time acting fuses that allow a physical break in the circuit if a short circuit arises, eliminating the need for a circuit reset. The thin
-more-
film design allows customers to order customized thin film chip fuses to meet their specific product needs. The Bourns SinglFuse line is also RoHS compliant and halogen free. 

“With the introduction of the new SinglFuse line, Bourns is able to satisfy growing customer demand for a broader range of circuit protection solutions that meet specific standards requirements and solve application challenges,” said Brian Ahearne, Multifuse® technical marketing manager at Bourns. “Our customers benefit from the industry’s broadest line of circuit protection products backed by years of collective application expertise and support.” 

Bourns’ SinglFuse thin film chip fuses:

Product

Fuse Type

Footprint

Rated Current

SF-0402F Series

Fast Acting/SMD

1005 (EIA 0402)

500 mA – 4.0A

SF-0603F Series

Fast Acting/SMD

1508 (EIA 0603)

500 mA – 5.0A

SF-1206F Series

Fast Acting/SMD

3216 (EIA 1206)

500 mA – 7.0A

SF-0402S Series

Slow Blow/SMD

1005 (EIA 0402)

500 mA – 4.0A

SF-0603S Series

Slow Blow/SMD

1508 (EIA 0603)

500 mA – 5.0A

SF-1206S Series

Slow Blow/SMD

3216 (EIA 1206)

500 mA – 7.0A

Pricing and Availability
Bourns’ SinglFuse SF Series product line is available now in production quantities. As a pricing reference, the new thin film chip fuses are offered in the price range of $0.32 to $0.38 in 5,000 minimum quantities.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a