Search
Languages

Delivering an Enhanced High Inrush Current Limiter Solution, Bourns Unveils its POWrTherm™ NTC Thermistors Line

The seven POWrTherm™ model series' wide resistance ranges and multiple board disc diameter options enable customers to meet specific application and market needs

RIVERSIDE, Calif., May 30, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today unveiled its POWrTherm™ NTC Thermistor product line designed to deliver enhanced and efficient high inrush current limiting capabilities. The new line includes seven series, Models BN-LG05Y, BN-LG08Y, BN-LG10Y, BN-LG13Y, BN-LG15Y, BN-LG20Y and BN-LG25Y. These models offer a wide resistance range along with multiple board disc diameter options so that customers can select the right product for their specific application requirements and various market needs.

Bourns® POWrTherm™ NTC Thermistors features unique construction which utilizes various metal oxides to form the polycrystalline NTC thermistor bodies that provide superior capabilities in suppressing high inrush currents. The seven POWrTherm™ series offer equivalent capacitance up to 1500 μF@240 VAC and a maximum current up to 15 A. In addition, the new model families are housed in radial leaded through-hole packages and are UL and/or TÜV recognized depending on the specific series. The new line is also available in different disc sizes to meet various market segment requirements from consumer to industrial, for applications such as Switched-Mode Power Supplies (SMPS), DC motors, amplifiers and transformers.

"At Bourns, we have extensive power protection expertise, and set out to provide a different and efficient technology approach to suppress inrush current with our POWrTherm™ Power NTC Thermistor products," said Shawn Yu, product line manager at Bourns Protection Division. "Our new POWrTherm™ NTC Thermistor solutions utilize the high initial resistance of negative temperature coefficient characteristics to effectively control and minimize unwanted inrush current. This feature proves beneficial in mitigating the potentially harmful effects of excessive current at startup. Additionally, during regular operation, the resistance of our POWrTherm™ devices significantly decreases, allowing for improved efficiency across a wide range of applications. As power demands continue to grow in modern end products, achieving enhanced efficiency has become increasingly critical."

All seven Bourns® POWrTherm™ NTC Thermistor Series protectors are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/ntc-thermistors

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com