Search
Languages

Bourns Launches Precision Wirewound Resistor Line Engineered to Meet High Accuracy and Long-Term Stability Application Requirements

Matching demanding application needs, new rugged resistors offer wide resistance values and are available in multiple package sizes and lead configurations

RIVERSIDE, Calif., October 28, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today launched its Riedon™ Precision Wirewound Resistor Series by Bourns. Engineered for high accuracy and long-term stability, these latest resistors offer a broad resistance range of up to 6 megohms (MΩ) with ultra-low resistance tolerances (±0.005 percent). This rugged, high-precision resistor series is housed in multiple axial, radial and square package sizes and is available in a variety of lead configurations, giving designers additional flexibility.

Bourns® new wirewound resistors feature non-inductive multi-Pi cores, protective encapsulation technology and an exceedingly-low standard temperature coefficient of ±2 ppm/°C. These features help minimize inductance and noise while maintaining stability and efficiency even under high heat and harsh electrical conditions. In addition, the series is 100 percent acceptance tested. An expansive variety of applications can benefit from these new precision wirewound resistors, including measurement equipment, bridge circuits, load cells and strain gauges, imaging systems, current sensing equipment and high-frequency circuit designs.

“The addition of the Riedon™ Precision Wirewound Resistors by Bourns as part of our expanding portfolio demonstrates our commitment to support demanding applications with products that deliver low TCR, tight tolerances, and strong pulse performance,” said Walter Garcia, Resistive Product Line Manager at Bourns. “We also offer the ability to customize these solutions to exacting customer requirements, helping them provide long-term value in critical designs that must meet elevated precision and reliability specifications.”

The Riedon™ Precision Wirewound Resistor Series by Bourns are available now, and are RoHS* compliant. For additional information, please see: bourns.com/products/resistors/precision-wirewound-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com