Search
Languages

Bourns Expands its Multifuse® Polymer PTC Resettable Fuses with Nine New High Temperature Products

The latest additions to the Model MF-USHT family broaden the hold current range, raise the maximum voltage and increase the operating temperature range up to +125 °C

RIVERSIDE, Calif., January 13, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the Company has expanded its Multifuse® Model MF-USHT Surface Mount PPTC Resettable Fuse Series with nine new products. These latest additions are AEC-Q200 compliant and broaden the hold current (Ihold) range up to 2.0 A and increase the maximum voltage (Vmax) to 36 VDC while raising the maximum operating temperature up to +125 °C.

The new fuses within the Model MF-USHT Series employ Bourns’ innovative freeXpansion™ technology, which enhances the product’s performance by incorporating higher hold currents, elevated voltages, and greater resistance stability all in a more compact footprint. These advanced features are particularly well-suited for overcurrent and overtemperature protection in electronic equipment that need to operate at high temperatures.

The nine new part numbers added to the Bourns® Model MF-USHT Series PPTC Resettable Fuse family are available now and are RoHS* compliant. In addition, the products are UL/CSA/TÜV recognized to meet safety criteria. The TÜV certifications also cover certifications for IEC 62319-1 and IEC 60738-1, as well as IEC 60730-1:2013 clause 15, clause 17, and Annex J. These products are manufactured within a Bourns IATF 16949 certified facility. For more detailed product information, please see: www.bourns.com/products/circuit-protection/resettable-fuses-multifuse-pptc#smdhts.

“Multifuse” is a registered trademark of Bourns, Inc. in the U.S. and other countries.

“freeXpansion” is a trademark of Bourns, Inc.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com