MENU
Search
Languages

Bourns Adds 250 Amp Series to its Digital Current Sensor Line Broadening Range of Measurement Solutions for Battery Applications

The Riedon™ Model SSD-250A Current Sensor – Digital by Bourns is a precise, compact, cost-effective measurement solution with the added benefits of digital

RIVERSIDE, Calif., January 7, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that it has further expanded its digital shunt sensor line with the release of the Riedon™ Model SSD-250A Series Current Sensor – Digital by Bourns. The new 250 amp series is available in two versions: the RS-485 serial interface model, which can also be configured as MODBUS RTU, and a customizable CANbus model. Designed to give developers a broader range of measurement solutions with the benefits of digital, this series features 100 A, 250 A and 500 A nominal current, a -40 °C to +115 °C operating temperature range and 1500 VDC galvanic isolation that helps to enhance accuracy and operational stability.

Offered in a compact System-in-Package (SIP), the Model SSD-250A Series delivers calibrated and temperature-compensated digital output, making these shunt sensors ideal current sensing solutions for a wide variety of battery-related applications including renewable energy systems, motor drives and EV charging stations. These shunt-based sensors also help eliminate the need for periodic device calibrations, all while providing highly accurate measurements that contribute to more efficient use of power. In addition, the new series features considerably lower insertion resistance than passive shunt sensors and Hall Effect sensors.

The Riedon™ Model SSD-250A Series Current Sensor – Digital by Bourns is available now, and is RoHS* compliant. For additional information, please see: www.bourns.com/products/sensors/current-sensors.

About Bourns

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.