MENU
Search
Languages

Bourns Introduces Industry’s First 240 V/1 kA Bidirectional Power TVS Diode in a Surface Mount Package

Compact, high power density protection meets growing requirement in applications with high-voltage DC bus architectures

RIVERSIDE, Calif., August 29, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today further demonstrates its innovation and technology leadership with the introduction of the industry’s first 240 V/1 kA Bidirectional Power TVS (PTVS) Diode that offers the highest power density available in a surface mount package. The Bourns® Model PTVS1-240C-M PTVS Diode is designed with advanced silicon processing technology that yields exceptionally high voltage-handling capabilities, and along with the diode’s surface mount packaging, differentiates this transient voltage protector into a league of its own.

Offering 1 kA surge handling capability under 8/20 µs test conditions, the Bourns® Model PTVS1-240C-M is ideally suited for a broad variety of systems that employ high-voltage DC bus architectures. These systems commonly experience high current switching transients and dynamic load behaviors where snubbing is needed or protection of bus-powered subsystems is required.

Bourns® Model PTVS1-240C-M PTVS Diode is a low-leakage device consuming only 10 µA in standby while delivering a maximum breakdown voltage of 295 V, repetitive standoff voltage of 240 V and precise clamping voltage of 340 V. Under 10/350 µs conditions, this device is rated for 200 A peak current, and its voltage breakdown sensitivity over temperature is an extremely linear 0.1 %/°C. The surface mount package offers a significant reduced PCB footprint and lower inductance design advantages compared to traditional through-hole mounted Power TVS Diodes.

Applications that can benefit from the features and capabilities of the Model PTVS1-240C-M include industrial power systems, motor controllers and inverters, solar inverters, battery energy storage systems, and factory automation.

The Bourns® Model PTVS1-240C-M is available now, is UL497B certified and meets IEC 61000-4-5 standard specifications. It is also RoHS* compliant and halogen free**. For additional information, please see: www.bourns.com/products/diodes/power-tvs-diodes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.