MENU
Search
Languages

Bourns Announces AEC-Q200 Compliant Gas Discharge Tube Series for Enhanced Reliability in Demanding Environmental Applications

Bourns® Model 2027-A Series features a high surge current rating that helps designers meet increased reliability, durability, regulatory standards and electrical performance goals

RIVERSIDE, Calif., July 31, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its latest AEC-Q200 compliant Gas Discharge Tube (GDT) family. The Bourns® Model 2027-A Series GDTs are designed to meet market demands relating to AEC-Q200 compliance in terms of reliability, durability, regulatory standards, electrical performance and additional advanced capabilities needed in certain harsh environmental applications. The stringent testing required by this standard makes the Model 2027-A Series GDTs ideal surge protection solutions for demanding applications such as photovoltaic installations, power supplies, low to medium risk medical devices**, HVAC, lighting, and IEC 62368-1 compliant equipment.

The Model 2027-A Series features 75 V - 600 V breakdown voltages, a high surge current rating and high insulation resistance with a wide -40 °C to +125 °C operating temperature range that offers superior thermal stability for applications that must operate in extreme temperature environments. With its high surge capability, Bourns’ latest GDTs can withstand high-energy transients, effectively protecting sensitive electronics from damage. Engineered for longevity, these new components help ensure sustained performance over the protected device lifespan, thereby helping to reduce maintenance and replacement costs.

"We designed our new AEC-Q200 compliant GDT series specifically for harsh environmental applications," said David Chavarría, GDT/SPD Product Line Manager at Bourns. "This family not only meets the stringent demands of AEC-Q200 compliance, but also opens new opportunities for [Bourns] to explore other markets where the highest level of protection is paramount to maximize system reliability and durability. As leaders in the development of advanced protection solutions, Bourns remains committed to continued innovation and delivering exceptional quality products for our customers worldwide."

Bourns® Model 2027-A Series 2-electrode AEC-Q200 compliant GDTs are available now and are RoHS compliant* and UL recognized. For more detailed product information, please see: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/standard-surface-mount-(smd)-2-electrode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.