Search
Languages

Leveraging the Benefits of its Advanced Metal Alloy Powder Core Process, Bourns Unveils High Current Shielded Power Inductors

Ideal for power management/EMI filtering, the miniature sized AEC-Q200 compliant power inductors offer high rated current, low radiation and a wide temperature range

RIVERSIDE, Calif., June 6, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today unveiled its latest high current shielded power inductors. The five series are designed using the company's advanced metal powder core and manufacturing processes, delivering the benefits of magnetically shielded construction for low radiation, high saturation current, high heating current and low DC resistance. The new power inductors, designated model SRP2010TMA, SRP2012TMA, SRP2510TMA, SRP2512TMA and SRP3212A series, are AEC-Q200 compliant and offered in a miniature, low profile 0.8 x1 mm design.

Ideal solutions for power conversion and EMI filtering in consumer, industrial and a variety of other electronics applications, Bourns' new high current shielded power inductor series are constructed with high temperature-graded materials providing excellent temperature stability and an operating temperature of up to +150 ºC. In addition, the inductors' flat wire construction helps significantly reduce DCR resistance compared to other similar-sized devices constructed with traditional wire while also making them highly efficient.

Bourns® high current shielded power inductor model SRP2010TMA, SRP2012TMA, SRP2510TMA, SRP2512TMA and SRP3212A series are available now and are RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com