MENU
Search
Languages

Bourns Announces Two Thick Film Resistor Series that Deliver High Power Dissipation in Compact TO-220 and DPAK Packaging

Riedon™ Model PF2203/PFS35 Series High Power Thick Film Resistors by Bourns dissipate up to 35 W of power with low TCR and tolerance options

RIVERSIDE, Calif., November 18, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns. Adding to Bourns’ broad high-power resistor line, the two series are available in compact TO-220 and DPAK packages, offering low inductance, excellent pulse handling capabilities, and elevated power ratings of 35 W that enable enhanced circuit stability and measurement accuracy.

The Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns feature a wide resistance value range from 10 Megohms to 51 Kiloohms, have a temperature range of -55 to +175 °C and are available with resistance tolerance options of ±1 percent and ±5 percent. Bourns is offering these resistors to match market demands for greater power dissipation in smaller packages. Surface mount packaging, such as the DPAK offered with the Model PFS35 Series, is also particularly popular for its ability to help reduce manufacturing costs.

The features of these thick film resistors make them ideal solutions to meet current limiting, current measurement, and capacitor discharge requirements in a broad variety of applications, including industrial motor drives, AC-DC and DC-DC power converters, and Battery Energy Storage Systems (BESS).

The Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns are available now, and are RoHS* compliant. For additional information, please see: www.bourns.com/products/resistors/high-power-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.