MENU
Search
Languages

Bourns Introduces Ultra-Low Capacitance TVS Diode Surge Protection Solution for Gigabit Ethernet Ports


Bourns® Model CDDFN10-2574N
TVS Diode Array (Click for JPG)

RIVERSIDE, Calif., August 8, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a TVS diode array designed to provide effective surge protection in high-speed communication port and sensitive transceiver applications. The Bourns® Model CDDFN10-2574N TVS diode array features a DFN10 package that uses a flow-through layout to enable minimal impedance change, which is a critical requirement for high-speed ports such as Gigabit Ethernet (GbE). Furthermore, its ultra-low capacitance of only 1.7 picofarads minimizes signal degradation on each channel.

The expanded adoption of sensor-based and Internet-of-Things (IoT) applications will continue to depend upon GbE and other high-speed lines. When these connected devices are deployed in remote, harsh environment locations, they are particularly susceptible to electrostatic discharge (ESD) and surge damage, and therefore, require robust protection. Offering a superior performance solution, Bourns' latest TVS diode array offers lower clamp voltage on surge, and unlike competing technologies, it uses solid-state avalanche technology that does not degrade after multiple ESD events.

The Bourns® Model CDDFN10-2574N TVS diode array combines a 2.5 V TVS diode with steering diodes to provide protection for eight high-speed data lines. It also meets specified safety standards providing ±30 kV contact and discharge ESD protection per IEC 61000-4-2, and 45 A (8/20 μs) IEC 61000-4-5 lightning protection.

Available now, the Bourns® Model CDDFN10-2574N surface mount TVS diode array is RoHS compliant*. As a pricing reference, it is priced at $0.60 in 12,000 pcs quantities. For more detailed product information, please see the datasheet: www.bourns.com/docs/Product-Datasheets/CDDFN10-2574N.pdf

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

**Bourns follows the prevailing definition of "halogen free" in the industry. Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.