Search
Languages

Bourns Maintains Leading AEC-Q200 Component Supplier Position with Introduction of Semi-Shielded and Shielded Power Inductor Series

Bourns’ AEC-Q200 Certified Semi-shielded Power Inductors
Click to enlarge (477 KB)

RIVERSIDE, Calif., ​September ​6, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a broad new series of automotive-grade semi-shielded and shielded power inductor components. Bourns offers one of the industry's broadest portfolios of AEC-Q200-qualified products consisting of resistors and magnetics that condition and filter electronic circuits, and circuit protection products designed specifically for automotive applications. AEC-Q200 is a global automotive standard for passive components to ensure temperature, pressure resistance and safety consistency. Along with the entire line of Bourns' automotive-grade components, the nine new inductor series have been tested and qualified to the AEC-Q200 specification, and are manufactured in facilities that are fully certified to TS 16949.

"Based on specific requests from our automotive market customers for semi-shielded inductors, the products were developed and tested, and are being manufactured according to strict AEC-Q guidelines in TS certified factories,” said Guido Zehnder, product line manager at Bourns, Inc. "Automotive designers can be assured of a component that has passed very clear defined specifications with dedicated controls.”

Bourns released six new AEC-Q200-qualified semi-shielded power inductor series: SRN2010TA, SRN3012TA, SRN3015TA, SRN4012TA, SRN6045TA and SRN8040TA and three AEC-Q200-qualified shielded power inductor series: SRR1050A, SRU1063A and SRU8045A. These inductors have been designed to provide effective magnetic shielding with low radiation, feature extended temperature range (-40 to +125 °C) operation and offer cost-effective solutions compared to similarly-sized conventional ferrite shield inductors. These features make them ideal for applications where low noise operating environments are essential such as driver assistant devices, information/entertainment systems, lighting as well as DC/DC converters and power supplies.

Pricing and Availability
Bourns' new series of semi-shielded and shielded power inductor components are available now and are RoHS compliant*. As a pricing reference, the semi-shielded Model SRN3012TA is priced at $0.12 each in 10,000 piece quantities and the shielded Model SRR1050A is priced at $0.40 each in 10,000 piece quantities. For additional product specifications, please go to: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-qualified

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com