MENU
Search
Languages

Bourns Wins EE Awards Asia Top 2024 Discrete Component of the Year

Bourns PTVS2-xxxC-H High Current Bidirectional TVS Diode was selected for prestigious award

RIVERSIDE, Calif., December 17, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that its Model PTVS2-xxxC-H High Current Bidirectional TVS Diode has won the EE Awards Asia 2024 Discrete Component of the Year Award from AspenCore’s Taiwan/Asia team that represents its EE Times and EDN publication brands. The awards celebrate companies and individuals who have made significant advancements in the electronics industry. This year’s EE Awards Asia had more than 400 submissions from nearly 170 companies worldwide, competing across 36 categories.

The Bourns product was selected by a team of senior analysts along with a global community of users. The EE Asia Award was presented to Clement Shu, Vice President of Sales, Bourns Asia Pacific, on December 5 at the ceremony in Taipei, Taiwan. “This recognition highlights Bourns' exceptional performance, and is a testament to the dedication of our team and the trust placed in us by our customers and partners,” said Shu.

The Bourns® Model The PTVS2-xxxC-H TVS diode was singled out for the award based on its superior surge current handling capability, fast clamping response and low capacitance features. These features and the product’s robust design have made it an ideal protection solution for high-speed data lines and sensitive components in telecommunications, industrial and power applications that are vulnerable to transient voltage spikes and electrical surges. Protecting these critical electronic systems is vital to helping to ensure their longevity and reliability.

For more information about the 2024 EE Awards Asia, please see their website: www.eetasia.com/innovation-takes-center-stage-at-the-2024-ee-awards-asia-ceremony/.

 

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.