Leave a message
MENU
Search
Languages

Bourns® TLVR Inductors Deliver Extremely High Current Capabilities to Match Today's Data-Driven Application Performance Demands

Engineered with a dual-winding structure and low inductance, the Bourns® Model TLVR1005T and TLVR1105T Series provide fast transient response that can scale to CPU, FPGA and ASIC load requirements

RIVERSIDE, Calif., May 7, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its Model TLVR1005T and TLVR1105T Series. Bourns' new multiphase trans-inductor voltage regulator (TLVR) inductors deliver extremely high current capabilities, low inductance, and low DC resistance (DCR) that are designed to meet today's data-driven application performance needs. These types of applications have evolved in processing performance and now require the support of power bead inductors that can match their exceptionally high current specifications in the same, if not less, board space. Bourns® Model TLVR1005T and TLVR1105T Series multiphase TLVR inductors meet these requirements for servers, workstations, data centers, storage systems, and desktop computers, as well as in graphics cards and a variety of battery-powered systems.

A problem arises with traditional multiphase voltage regulators (VRs) in balancing performance, as high-current output demands require an increase in the duty cycle previously handled via long individual-phase stages. New multiphase TLVR architectures, developed to mitigate transient responses stemming from sudden increases in load output, are widely adopted to address these concerns. As such, system designers see the advantages of phase coupling in TLVR architectures, enabling extremely fast transient response, scalable with CPU, FPGA, and ASIC load requirements. The adoption of this architecture allows designers to develop robust systems without sacrificing other critical design parameters such as board space, system efficiency, power density, or BOM costs.

Engineered with a dual-winding structure and clip type coil, the Bourns® Model TLVR1005T and TLVR1105T Series deliver the low inductance and extremely high current capabilities (Irms up to 77 A and Isat up to 160 A) that are needed in a new generation of multiphase power solutions. The series' shielded construction offers low radiation with an inductance range of 70 to 200 nH and an operating temperature range of -40 to +125 ºC.

The Bourns® Model TLVR1005T and TLVR1105T Series are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-dual-winding-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.