Leave a message
MENU
Search
Languages

Bourns Announces 1210-Size Automotive Grade Common Mode Chip Inductors

New compact sized and rugged inductors feature low radiation and high impedance over a broad frequency range to provide excellent EMI suppression

RIVERSIDE, Calif., March 15, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its new 1210-size automotive grade common mode chip inductor series. Bourns' latest family of common mode inductors are designed with a ferrite core and are bifilar-wound to deliver a compact size and shielded construction. The Model SRF3225AB and SRF3225TAC common mode chip inductor series offer low radiation and high impedance over a broad frequency range to suppress Electromagnetic Interference (EMI) entering or leaving the system making them excellent solutions for design-in and testing in consumer, industrial and many other electronics applications.

The inductor core features a 0.2/0.3 mm height sidewall terminal at each end designed to help enhance the component's mechanical strength after it is assembled on the board. Both model series are AEC-Q200 compliant for higher reliability and durability. The Model SRF3225AB is specifically designed for noise suppression in 2-wire UTP (unshielded twisted pair) cable automotive audio bus systems. Designers will find the SRF3225TAC series well-suited for common mode noise suppression in typical CAN and higher data rate CAN-FD Class II applications.

The new Bourns® Model SRF3225AB and SRF3225TAC series are available now and are RoHS compliant* and halogen free**. For additional product information, please see: www.bourns.com/products/magnetic-products/common-mode-chip-inductors-aec-q200-compliant 

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.