MENU
Search
Languages

Bourns Announces New AEC-Q200 Compliant Thick Film Resistor Series Designed for General Purpose Applications

Available in 8 Compact Form Factors, New Resistors Are Space-Saving Solutions in Form Factors as Small as 0201 to Meet Downsizing Market Trends

RIVERSIDE, Calif., April 20, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new AEC-Q200 compliant series of thick film chip resistors. Bourns continues to take a leading role in introducing space-saving resistor products by offering its latest Model CRxxxxA series in eight compact form factors—from small 0201 (0603 Metric) up to 2512 (6431 Metric). The CRxxxxA series is part of the Bourns® CR line of general-purpose thick film chip resistors. Bourns designed this family of devices in five different versions to support specific application requirements: CR standard, CR-PF ultra-low lead content, CR-AS sulfur resistant, CRxxxxA-AS AEC-Q200 compliant and sulfur resistant and CRxxxxA AEC-Q200 compliant.

The CRxxxxA series features rated power from 0.05 to 1 watt and a wide resistance range from 1 ohm up to 20 megohms. These features make this series an optimal circuit conditioning solution for a broad range of consumer, industrial, telecom and other applications.

Bourns manufactures its latest resistors using a thick film element that is printed onto a ceramic substrate. This type of advanced ceramic substrate offers excellent heat dissipation. The resistive element is coated by an epoxy overcoat layer, which isolates the resistive element electrically to help protect it against mechanical damages and environmental effects such as humidity and gasses.

Available now, Bourns® Model CRxxxxA series is RoHS* compliant and halogen free**. For additional product information, please see: www.bourns.com/products/fixed-resistors/thick-film-chip-resistors

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.