Search
Languages

Bourns Introduces Low Capacitance TVS Diodes Designed to Protect High-Speed Interfaces in Automotive Applications

RIVERSIDE, Calif., May 22, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new TVS diodes series featuring low capacitance of 3 pF (picofarads) making them ideal protection devices for the high-speed interfaces found in today's automotive, communication line and industrial applications. The Bourns® Model CDSOD323-TxxC-DSLQ TVS diodes also offer the Bourns' lowest TVS diode leakage current of 1 nA (nanoampere). This is important as IoT sensors, vehicle sub-systems such as entertainment and comfort equipment have limited run-time determined by the battery. Using low leakage protection devices has the benefit of helping to improve power efficiency and extend run-times.

 

The Model CDSOD323-TxxC-DSLQ series provides ±30 kV contact discharge ESD protection per IEC 61000-4-2 and surge protection per IEC 61000-4-5. These features are designed to improve the reliability and increase application robustness against damage from ESD and other transient voltage events. The new TVS diodes from Bourns are available in a SOD323 package with bidirectional TVS offering superior protection especially for communication lines.

The series includes two new AEC-Q101 compliant surge protection models: Model CDSOD323-T12C-DSLQ and Model CDSOD323-T24C-DSLQ. Both models are available now, are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/diodes/diodes-aec-q101-compliant.

* RoHS Directive 2015/863, Mar 31, 2015 and Annex.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com