MENU
Search
Languages

Bourns Kicks Off Significant Expansion of its SinglFuse™ Product Line with Five New Thin Film Series

RIVERSIDE, Calif., April 17, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, has announced the introduction of the first of many new SinglFuse™ product series the company has planned in its strategic roadmap for 2018. The significant expansion of its SinglFuse line will include advanced wire-core, ceramic multilayer and ceramic tube fuse technologies in addition to the company’s successful thin film chip fuse products. As a leading innovator of one of the industry’s most comprehensive offerings of circuit protection solutions, the planned increase in Bourns’ SinglFuse™ product families answers the growing need for robust and reliable overcurrent protection that meets designers’ higher-rated voltage (up to 600V AC) and higher-rated current (up to 100A) application requirements. Bourns will also roll out several new series of automotive-grade fuses later in the year.

 

The first of the new SinglFuse™ devices to be introduced are five new fast-acting precision and time-lag thin film fuse product series. Fast acting precision fuses are rated to open within 5 seconds at 200 percent rated current. Time lag thin film fuses open within 1 to 120 seconds at 200 percent rated current. These latest fuse products from Bourns address the increasing need for effective circuit protection in applications including PC and LCD monitors, portable memory, cell phones, digital cameras and set-top boxes.

The first five new SinglFuse™ product series include Models SF-1206FP, SF-1206SP, SF-0603FP, SF-0603SP and SF-0402FP. These single blow fuses for overcurrent protection feature current ranges from 500 mA to 7.0 A. Offered in surface mount packaging for automated assembly, these new products also help meet limited design space constraints with small, industry-standard 0402 (1005 metric), 0603 (1608 metric) and 1206 (3216 metric) footprints.

All five of the new SinglFuse™ product series are RoHS compliant*, halogen free** and available now. For more information, please visit the product page: www.bourns.com/products/circuit-protection/singlfuse-smd-fuses or contact your local Bourns Representative or Authorized Distributor.

* RoHS Directive 2015/863, Mar 31, 2015 and Annex.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.