Search
Languages

Bourns New Trimming Potentiometers Offer Significantly Lower CRV and Improved Linearity for Sensitive Microprocessor Designs

RIVERSIDE, Calif., September 27, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced high reliability precision Trimpot® trimming potentiometers that provide more accurate linearity, lower Contact Resistance Variation (CRV) and can be customized to a customer's exact requirements. Based on the company's continued innovation and 70-year history of engineering, Bourns designed its new precision Trimpot® products for use with microprocessors or in applications where precise adjustment is needed.

Newer circuit designs that incorporate microcontrollers are more sensitive to noise. In order to read all output correctly, tighter linearity and less noise have become critical requirements when precise, accurate design adjustment settings are needed. Bourns new generation of precision Trimpot® products offer a more consistent ratio of output (electrical reading) to input (mechanical rotation) to meet strict linearity requirements. Their lower CRV means less noise that results in fewer output errors. Designers also gain the ability to offer faster operator and machine adjustments to the target resistance while providing a more consistent output curve.

Customers can place orders immediately for Bourns' sealed, multiturn precision Trimpot® products in 6 mm through-hole or 4 mm surface mount (SMT) packages. The new products are RoHS compliant* and can be ordered halogen free**. For more detailed customization and ordering information, please contact: techweb@bourns.com

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com