Search
Languages

Two Bourns Products Win 2025 EE Awards Asia in the Discrete Component Category

Bourns® Planar Transformer took the discrete award in the Taiwan region and Bourns® SRP Series Shielded Power Inductors earned the Asia region award

RIVERSIDE, Calif., December 5, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that two of its products have won the 2025 EE Awards Asia in the discrete component category.

  • Bourns® Planar Transformers won the award in the Taiwan region, recognized for its compact, low-profile design with planar copper foil windings that deliver superior thermal performance and higher efficiency in a compact footprint. These transformers are excellent solutions for automotive on-board chargers and DC-DC converters.
  • Bourns® SRP Series Shielded Power Inductors won the award in the Asia region, and were singled out for their ultra-low DC resistance, strong magnetic shielding and high saturation current. These AEC-Q200 qualified inductors offer enhanced reliability and are particularly well-suited for broad applicability in automotive, telecom, and consumer electronics.

“The winning of these two prestigious awards shows the beneficial component advancements Bourns engineering has achieved in meeting ongoing power electronics requirements,” said James Harrington, Senior Vice President Worldwide Sales at Bourns, Inc. “These wins also recognize what can be accomplished with dedication and a commitment to excellence from the entire Bourns team. I congratulate all those responsible, and know they continue to be inspired to drive innovation that propels ever-greater designs.”

The EE Awards Asia acknowledge companies and individuals who have made significant advancements in the electronics industry and are bestowed by AspenCore’s Taiwan/Asia team that represents its EE Times and EDN publication brands. The award ceremony was held at the Grand Mayfull Hotel in Taipei, Taiwan on December 5.

These Bourns products were selected by a team of senior analysts along with a global community of users. The EE Asia Award was presented to Edward Liu, Product Line Director, Magnetics Components, on December 5 at the ceremony in Taipei, Taiwan. “This recognition highlights Bourns' exceptional performance, and is a testament to the dedication of our team and the trust placed in us by our customers and partners,” said Liu.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com