Search
Languages

Bourns Releases Four New Foil Resistor Series Designed for High-Precision, High-Power Applications

The Riedon™ FPM, FPV, FWP2324 and FPY Series Foil Resistors by Bourns deliver long-term measurement repeatability and help reduce calibration frequency

RIVERSIDE, Calif., December 2, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released four new Riedon™ Foil Resistor Series by Bourns. The FPM Series, FPV Series, FWP2324 Series and FPY Series are designed for high-precision, high-power applications by delivering exceptional accuracy and long-term measurement repeatability. These capabilities enable designers to meet stability, performance, high power and reliability requirements while also helping to reduce calibration frequency even in certain harsh environments.

The four new foil resistor series can achieve up to 1 ppm/°C and ±0.005 percent TCR and minimal long-term drift. These resistors are constructed with a metal foil resistive element mounted on a ceramic substrate that provides superior heat conductivity. In addition, the metal foil resistive element also offers high precision, low inductance, low noise and enhanced long-term reliability.

The features offered in the Riedon™ FPM, FPV, FWP2324 and FPY Series Foil Resistors by Bourns make them ideal, long-life measurement solutions for a wide variety of current sense, industrial, consumer and telecommunications applications. In addition, their high precision and robust thermal performance make these foil resistors especially well-suited for test and measurement equipment, renewable energy and power conversion systems and industrial automation platforms, where consistent accuracy, stable performance over varying conditions and long-term reliability are essential.

Enabling designers to match individual application requirements, the new resistor families are available in the following package types :

  • The FWP2324 Series in a 4-pin, rectangular package
  • The FPY Series in a 2-pin, rectangular package
  • The FPM and FPV Series in a 4-pin package with an isolated backplate
The Riedon™ FPM, FPV, FWP2324 and FPY Series Foil Resistors by Bourns are available now and are RoHS* compliant. For additional information, please see: bourns.com/products/resistors/metal-foil-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com