Search
Languages

Bourns Releases Two Compact NTC Thermistor Series Offering High-Precision Temperature Sensing and Compensation

The Bourns® BTN02G and BTN04G Series provide essential and highly accurate thermal management for today’s sophisticated and sensitive electronics applications

RIVERSIDE, Calif., June 4, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its BTN02G and BTN04G Series SMD Negative Temperature Coefficient (NTC) Thermistors. Designed as a high-precision and compact temperature sensing and compensation solution, Bourns’ new NTC thermistors provide essential thermal management for today’s more sophisticated and sensitive mobile devices, home appliances, Li-ion battery packs, LCD displays and other electronic equipment.

These new thermistors feature resistance that is inversely proportional to the temperature, enabling accurate temperature measurement. The advanced and high reliability design of the BTN02G and BTN04G series combines semiconducting ceramics and internal electrodes, providing the capability to uniformly and smoothly change resistance values over a wide temperature range. In addition to the standard ±3 percent and ±5 percent high-precision resistance tolerances, Bourns’ latest NTC thermistors are also available in ±1 percent and ±2 percent resistance tolerances. The series’ B-Value tolerance is highly accurate at ±1 percent, making them superior temperature sensing solutions.

Bourns® BTN02G and BTN04G Series SMD NTC Thermistors are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/thermal-sensing-devices/ntc-thermistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com