MENU
Search
Languages

Bourns Next-Generation GDTs Deliver State-of-the-Art Performance, Improve Standard Surge Current Ratings by 40 Percent

New GDTs Engineered to be More Responsive and Robust Using Bourns' Advanced Computer Model Simulation Techniques

RIVERSIDE, Calif., January 11, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its gas discharge tube (GDT) Model GDT25 series that offers a 40 percent improvement in standard surge current ratings from existing Bourns® models. These new and improved next-generation devices have been designed using Bourns' proprietary, advanced computer simulation techniques and offer industry-leading maximum impulse voltage limiting specifications. The performance delivered in Bourns' latest generation GDT25 series helps to significantly heighten protection against induced voltage transients such as lightning and AC induction. Plus, the enhanced level of protection with tighter voltage limiting provided during fast-rising events should reduce stress on downstream components compared to current standard GDT designs.

Offering superior current handling capabilities, specific Bourns® GDT25 series models are available in several voltages that exceed the industry standard lightning surge current rating of 5 kA for a 5 mm surface mount GDT. In addition, these next-generation Bourns® GDTs provide excellent performance across a wide temperature range, low capacitance and low insertion loss making them an ideal protection solution for high-speed information and communication technology (ICT) equipment such as set top boxes, Ethernet, DSL and G.Fast-based applications.

"The speed and robustness we designed into our Model GDT25 series presents a new standard for 5 mm overvoltage surge arrestors, as demonstrated by featured ratings of 7 kA, 8/20 surge and 7 A AC with one second power cross. Our new GDT series continues our legacy of delivering the quality, innovation and engineering excellence customers have come to expect from Bourns," said Tomaz Bojko, Product Line Manager at Bourns.

Providing an additional protection solution design resource that will help engineers to streamline prototype testing, a Bourns® GDT25 Design Kit is also available that contains five pieces of each GDT25 model.

The Bourns® GDT25 series is UL recognized and available now. For more detailed product information, please see: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/standard-surface-mount-(smd)-2-electrode 

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

***Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
Firmenkontakt:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com