Search
Languages

Bourns New Model PSL Motorized Slide Potentiometers Contribute to Lower Profile Audio, Broadcast, and Lighting Console Designs

RIVERSIDE, Calif., January 5, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the company's new low profile motorized slide potentiometer line specifically designed to meet small space constraints, longer product life and repeated automated console adjustment requirements. Offered in 100 mm and 60 mm versions, the innovatively designed Bourns® Model PSL measures just 25 mm high, enabling audio, broadcast and lighting console engineers to reduce the surface height resulting in a slim and sleek console design.

Bourns will showcase its latest slide potentiometers and the advanced capabilities of its complete line of professional audio and lighting products at the upcoming 2018 NAMM Show, January 25-28 at the Anaheim Convention Center in Bourns booth # 12506.

With the Model PSL, Bourns is answering the current trend for lower profile solutions that also meet increased power efficiency demands while maintaining high performance characteristics. Bourns designed its latest motorized slide potentiometer with a power-saving 5 VDC Mabuchi motor so it can be used with more energy-efficient circuits. The new product line also utilizes a highly durable contacting carbon resistive ink element that delivers extended wear characteristics of up to 500,000 cycles. The element design also produces very low noise output for an optimal signal-to-noise ratio that allows improved audio quality.

Available in a variety of resistance values and standard taper options, the Bourns® Model PSL motorized slide potentiometers feature a touch sense lever, a servo track option for console automation and an easy-to-use snap-in connector.

As a pricing reference, the 100 mm version of the Model PSL is $24 in quantities of 1,000 pieces, and the 60 mm version is $23 in quantities of 1,000 pieces. Both versions are RoHS compliant* and available now through Bourns qualified distributors. For additional product information, please see the data sheet and material declaration at www.bourns.com.

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com