MENU
Search
Languages

Bourns Expands Innovative Line of Volume, Space-saving FLAT® GDT Devices

RIVERSIDE, Calif., October 17, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today expanded its standard-setting line of volume and space saving FLAT® gas discharge tube (GDT) surge arrestors. The Model 2018 Series FLAT® GDT is a 3-electrode device that delivers a low profile solution for high density and height-restricted PCB-based applications. The new series is lighter weight with a 50 % height reduction compared to standard 8 mm Bourns® GDTs. Bourns designed this latest series as a surface mount device with a large top flat surface, making it ideal for vacuum head pickup in today's high-speed pick and place manufacturing.

The Bourns® FLAT® GDT Model 2018 is an ITU K.12 Class III device rated at 20 kA¹ on an 8/20 µs waveform. The series is offered with DC breakdown voltages ranging from 90 to 500 V and features an innovative flat design that reduces the height of the Bourns® GDT from a typical 8 mm to a low profile of 3.5 mm.

"Besides saving valuable PCB space, these new 3-electrode FLAT® GDT devices help to reduce component count in space-constrained designs. The series provides the ability to protect both Line to Ground and Line to Line with a single Model 2018 FLAT® GDT, which previously required two GDTs," said Kurt Wattelet, product line manager at Bourns, Inc. "As a 3-electrode GDT, transverse voltage limiting performance is enhanced with the ability to share a common center electrode designed to allow both sides of the GDT to turn on quickly resulting in balanced operation."

Pricing and Availability

The new Bourns® FLAT® GDT Model 2018 Series is available now and is RoHS compliant*.  As a pricing reference, the Model 2018 Series is priced at $0.98 each in 100 piece quantities. For additional product specifications, please go to: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/3-electrode-gdts/flat-series-3-electrode

¹ Total current rating through center electrode, half value each line to center electrode.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.