Search
Languages

Bourns Announces Industry’s First Surface Mount Miniature Resettable Thermal Cutoff (TCO) Devices for Battery Cell Protection

RIVERSIDE, Calif., ​April 4, 2017 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the industry’s first surface mount Miniature Resettable Thermal Cutoff (TCO) devices. Bourns' new Model SA Series TCO battery protection solutions are compatible with surface mount reflow soldering methods, which eliminate supply chain steps and streamline the manufacturing process.

By controlling abnormal, excessive current virtually instantaneously up to rated limits, miniature TCO devices have become popular overcurrent and overtemperature protection solutions for lithium polymer and prismatic cell battery packs. TCO devices are traditionally welded in place in the manufacturing process. Bourns designed its new Model SA series so they could be soldered directly onto printed circuit boards saving manufacturing time and costs for battery cell suppliers.

The very low profile Model SA series has a maximum height of just 1.09 mm. They offer current capabilities from 6 A up to 11 A at 60 °C, are designed to withstand humid environments and offer high corrosion resistance from their bimetal mechanism. These features and their surface mount packaging make them ideal protection solutions for notebook PCs, tablet PCs and smart phones as well as open up new application areas such as USB Type C cables, automotive heating and power tools.

Pricing and Availability
Bourns’ new Model SA Series is available now, and a low current version is under development. These new TCO devices are also RoHS compliant* and UL recognized. As a pricing reference, the Model SA85SB0 is priced at $1.10 each for 7500 pieces.

For more information, please go to: www.bourns.com/products/circuit-protection/mini-breakers

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com