Search
Languages

Bourns to Present Magnetics Industry Session at APEC 2019

RIVERSIDE, Calif., March 4, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that a Bourns senior technical market manager will present an Industry Session entitled, "High-flux Density Nanocrystalline Materials for High-Frequency Power Applications" at the upcoming APEC 2019 Conference. The presentation was developed in conjunction with the Tyndall National Institute at the University College Cork in Ireland. It is part of the Magnetics session taking place on Thursday, March 21 from 8:30 to 11:25 a.m.

This topic is timely as power converter designers are interested in evaluating lighter and smaller inductors for high-frequency switching DC/DC converters. Recent advancements in cutting-edge efficient power switches at high frequencies have enhanced the need for miniaturized magnetic components in the power semiconductor industry. Therefore, new core materials breakthroughs are needed to enable more compact high-power inductor designs that offer stable inductance values, minimal core losses and improved performance.

Bourns will also display its broad portfolio of power conversion and power protection components for power electronics applications at APEC 2019 at the Anaheim Convention Center, March 17 – 21 in booth #774. More information about the Industry Sessions at APEC 2019 can be found at www.apec-conf.org/industrysessions.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com