Search
Languages

Bourns' Latest Overtemperature Protection Mini-Breaker Device Series – Automotive Grade and AEC-Q200 Compliant^

Bourns® Model AD and SD Series meet automotive industry's exacting requirements, and its manufacturing facility is IATF 16949 certified and passed VDA 6.3

RIVERSIDE, Calif., July 25, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that its Model AD and SD Series Miniature Thermal Cutoff (TCO) mini-breaker devices have received automotive grade approval and are compliant to AEC-Q200 equivalent standards^. In addition, Bourns' mini-breaker manufacturing facility is IATF 16949 certified and has passed the VDA 6.3 process audit requirements. As surface mount, ultra-small overtemperature protection devices, Bourns® automotive grade mini-breakers create an extra level of temperature monitoring safety and warranty confidence for automotive application developers and users alike.

These two latest mini-breaker device series have multiple industry-leading features that deliver the advanced level of resettable, accurate and repeatable overtemperature protection automotive designers can leverage in a broad range of heater circuit-based applications. They are available in several mounting options – the Model SD Series comes in a surface mount package, and the Model AD Series in an axial leaded/weldable package. Both series offer non-automatically resettable (self-hold) or automatically resettable (non-self-hold) function options, and feature a very wide trip temperature range of 55 °C to 150 °C.

"Now that we offer automotive grade products, our Model AD and SD Series mini-breakers give developers peace-of-mind that Bourns has all the competencies to support the wider automotive industry," said Brian Ahearne, Thermal & Precision Division Vice President at Bourns. "Although existing solutions offer the ability to monitor temperature, there are still inherent risks. Bourns® Model AD and SD Series provide independent overtemperature protection where the devices can be located in immediate contact with the heat generating components, either SMD or welded. Plus, their miniature package size and wide trip temperature range makes them ideal for heater circuits that formerly did not have overtemperature protection, or had to use bulky traditional solutions."

Bourns® Model AD and SD Series mini-breakers are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/mini-breakers

^Tested to Bourns internal AEC-Q200 equivalent standards

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com