Search
Languages

Bourns Introduces Photovoltaic (Class gPV) Power Fuse Product Series

The first two series of the Bourns® POWrFuse™ High-Power Fuses family feature high power ratings and are designed to UL 248 and IEC 60269 standards

RIVERSIDE, Calif., June 16, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced the first two series of its POWrFuse™ High-Power Fuse product family. Featuring a high-power rating, Bourns' new industrial fuse links are designed to UL 248 and IEC 60269 standard requirements. The capabilities of the POWrFuse™ series help protect solar photovoltaic power systems known to operate under extreme ambient temperatures, high-cycling and low-level fault current conditions. They are also excellent solutions for a variety of industrial, power supply and Battery Management System (BMS) applications.

Specifically, the POWrFuse™ PF-E series is designed to the UL 248-19 (Class gPV) photovoltaic fuse standard and offers 1000VDC voltage, power ratings from 15 to 30 A, and up to a 20 kA interrupting rating. The POWrFuse™ PF-H (gPV) series is designed to the UL 248-19 and IEC 60269-6 (Class gPV) photovoltaic fuse standards and offers 600VDC/VAC voltage, power ratings from 15 to 30 A, and up to a 150 kA interrupting rating. Both high-power fuse series offer fast-acting protection under fault current, low resistance and power loss, and an operating temperature range of –55 to +125 °C. Ferrule and PCB mounting options are available for both series.

The Bourns® POWrFuse™ PF-E and PF-H (gPV) series are available now and are RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/fuses/powrfuse-high-power-fuses

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com