MENU
Search
Languages

Bourns Expands Line with Three New Semi-Shielded Power Inductor Series Featuring High Operating Temperature

New power inductors are AEC-Q200 compliant and meet high-reliability requirements in EMI filtering, DC-DC converter and power supply applications

RIVERSIDE, Calif., February 24, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the expansion of its power inductor line with three new semi-shielded power inductor model series, Model SRN3030HA, SRN4030HA, and SRN5030HA. The new AEC-200 compliant power inductors from Bourns are designed with high current capacity, compact size, low loss, high operating frequency, and high operating temperature. The high temperature-graded materials employed in all three series achieve a 150 °C operating temperature rating and provide a wide operating temperature range of –55 to +150 °C. These features and capabilities make Bourns’ latest power inductors ideal, high reliability power conversion solutions for EMI filtering, DC-DC converters and power supplies in consumer, industrial, and telecom electronics.

A magnetic-silica based coating applied to the perimeter of the inductor winding enhances the inductors’ shielding and reduces magnetic field radiation compared to non-shielded options. Additionally, semi-shielded construction contributes to a lower component cost compared to similarly-sized conventional ferrite-shielded inductors. Each series offers different heating current ratings with saturation currents from 5 A to 10 A. Both Model SRN3040HA and SRN4030HA series have inductance ranges of 1-100 μH, and the SRN5030HA has a range of 0.47-100 μH. High Q values of 13 to 33 are possible in these compact power inductors, which provide high impedance at resonance frequency in combination with low loss operation.

Bourns® Model SRN3030HA, SRN4030HA, and SRN5030HA power inductors are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.