Search
Languages

Bourns Introduces Shielded Gigabit Ethernet/PoE+ Chip LAN Transformers for High-Speed Telecom and EMI Suppression

Two new low profile model series provide PCB layout flexibility and support Ethernet speeds up to 10 Gbps with PoE+ capabilities

RIVERSIDE, Calif., December 20, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, , today introduced two new shielded Gigabit Ethernet (GbE) Chip-LAN Transformer series. Bourns® Model SM453230-121N7YP and Model SM453230-231N7YP series are small, low profile and discrete solutions giving designers additional board layout flexibility compared to traditional Chip-LAN modules. In addition, Bourns' new transformers support high network speeds up to 10 Gbps, are capable of 700 mA for PoE+ and offer a temperature range of –40 to +85 °C. They are capable of 1500 VAC/60 s Hi-Pot isolation and withstanding pulse voltages of up to 2400 V, 1.2/50 μs. These advanced features make them ideal for use in high-speed telecommunication and networking devices.

The two transformers differ in inductance, insertion loss and capacitance features due to the different bit rate ranges they address. Bourns® Model SM453230-231N7YP supports 1, 2.5 and 5 GbE, whereas Model SM453230-121N7YP is 10 GbE capable. The former can be paired with Bourns® Model SRF2012A-801Y common mode chip inductor, and the latter with Model SRF2012-900YA. These small, center-tapped transformers are wound on a drum core and capped with a ferrite plate to emulate the close magnetic path of a toroid core. A center tap allows for common mode suppression even without an extra common mode filter, and the new series help reduce EMI troubleshooting efforts.

Bourns utilizes its fully automated production process for both new model series, which enhances component uniformity, quality and reliability. Also, high-volume production can be accommodated with shorter production lead times and reduced cost with this process.

Bourns® Model SM453230-121N7YP and SM453230-231N7YP GbE Chip-LAN transformers are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/transformers-signal

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com