Search
Languages

Bourns Announces New Automotive Grade, AEC-Q200 Compliant Common Mode Choke Series for DC Power Line Applications

The compact, low-profile Model SRF7035A Series meets board space constraints providing EMI suppression and noise filtering on high voltage/current DC power lines

RIVERSIDE, Calif., November 15, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its new automotive grade, AEC-Q200 compliant SRF7035A Common Mode Choke Series designed to support high voltage and current in DC power line applications. There are five impedance ratings with voltages up to 80 VDC and current up to 5 A. This gives designers additional flexibility and also expands the use for compact common mode filters in power applications. This rugged, compact and low-profile series is offered in a surface mount package and is a drop-in replacement for similarly-rated solutions. As board space constraints drive component profile and footprint minimization, an option now exists for a compact surface mount design common mode filter for DC power lines.

The SRF7035A Series common mode chokes feature a wide operating temperature range of -40 °C to +125 °C, rugged shielded construction for low radiation, a special rectangular-shaped ferrite ring core for reduced noise, and H-class enameled wire for high temperature capability. These features make the series an optimal choice for electromagnetic interference (EMI) suppression and noise filtering on DC power lines in DC-DC converters, switch-mode power supplies and power systems for automotive, consumer, industrial and other electronics markets.

The new series also offers windings in a segment-wound configuration that provides high common mode impedance over a broad frequency range and increased differential mode impedance above 100 megahertz (MHz). Bourns' latest common mode chokes deliver superior strength to meet various mechanical stresses via the device's clamping U-shaped terminals. A protective plastic shield covers the choke's surface and wires and separates N1 and N2 windings, allowing a Hi-Pot capability of 500 VAC at 3 mA for 1 sec. Rated at 80 VDC, the SRF7035A Series is ideal for next-generation applications where DC voltage is shifting from 12 V to 24 V and 48 V.

Bourns® Model SRF7035A Common Mode Choke Series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokes

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com