MENU
Search
Languages

Bourns Unveils AEC-Q200 Compliant Shielded Power Inductor Series Designed to Meet High Current Density, High Temperature Requirements

Model SRP6530A shielded power inductors feature high saturation current, low radiation and low buzz noise over wide –55 °C to +155 °C operating temperature range

RIVERSIDE, Calif., August 9, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released its Model SRP6530A Shielded Power Inductor Series designed to meet the high current density and high temperature requirements in a variety of applications. These AEC-Q200 compliant inductors feature shielded construction with a metal alloy powder core that offers low magnetic field radiation, low buzz noise, and a wide operating temperature range of –55 °C to +155 °C. The features of the Model SRP6530A series make them ideal for electromagnetic interference (EMI) filtering and power management solutions in consumer, industrial, and telecom electronics applications that require higher reliability.

Bourns' uniquely-formulated metal alloy powder core and molded construction offer high saturation currents of 7 to 70 A over the 0.1 – 10 μH inductance range. The new inductors provide low DC resistance, which enhances their low loss characteristics. In addition, the high temperature-graded materials used by Bourns enable a wide operating temperature range with a 50 VDC rating and high rated currents up to 34 A. The new inductor series also offers excellent temperature stability of inductance across a wide temperature band.

Bourns® Model SRP6530A shielded power inductor series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.