MENU
Search
Languages

Bourns Announces Low Profile, Highly Robust Common Mode Chokes with High Current Capacity for Power Applications

New Common Mode Chokes Deliver Common Mode and Differential Mode in a Single Surface Mount Design Suitable for DC Power Line Applications

RIVERSIDE, Calif., December 9, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced two new low-profile, high current series of compact surface mount common mode chokes. The new SRF1206A and SRF9045A series provide not only common mode but also differential mode filtering in a single choke configuration. These highly robust products offer high current capacity to answer the need for components that meet board space constraints in an increasing number of DC voltage domain applications with voltages up to 80 VDC and currents up to 8 A. This feature makes Bourns' latest common mode chokes excellent solutions for DC-DC converters, switch-mode power supplies, battery management and power line noise suppression in consumer, industrial and other electronics applications.

The SRF1206A and SRF9045A series are AEC-Q200 compliant with operating temperature ranges from -40 to +125 °C, and provide high impedance over a broad frequency range to suppress electromagnetic interference (EMI) either coming into or out of systems. Both series of common mode chokes use separate sector-wound winding configurations, and feature U-shaped terminals clamped to core for superior strength to handle various mechanical stresses. These series also feature a protective plastic shield that protects the part's surface and wires and enables Hi-Pot capability of 500 VAC @ 3 mA, 1 second. In addition to the normal common mode impedance that these components are designed to achieve, this construction also features increased differential mode impedance at a high frequency range.

Bourns® SRF1206A and SRF9045A series are available now, and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant 

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.