Search
Languages

Bourns Introduces AEC-Q200 Qualified Power Inductor Products Offering Exceptionally Low Resistance, High Saturation Current

RIVERSIDE, Calif., October 5, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced three new series of AEC-Q200 qualified high current shielded power inductor products. The Bourns® Models PQ2614BLA, PQ2614BHA andPQ2617BHA are designed with a flat wire winding offering exceptionally low DC and AC resistance and high saturation current of over 100 A. The flat wirewound design also provides a compact, highly efficient inductance solution. These features make the new inductor products particularly well-suited for automotive power conversion applications as well as DC/DC converters, switch-mode power supplies and filtering applications in consumer, industrial, medical and communications electronics.

Boosting the overall efficiency of DC/DC converters, these inductors feature low power dissipation combined with the low core loss nature of their ferrite core construction. In addition, these devices are mounted on a plastic base designed with an extra solder pad for increased mechanical stability. The series are offered with extended operating temperature ranges from -40 to +155 °C and inductance values of 1 - 33 µH.

The Bourns® Model PQ2614BLA, PQ2614BHA andPQ2617BHA series are available now and are RoHS compliant* and halogen free**. As a pricing reference, the Bourns® Model PQ2614BLA is priced at $1.80 each in 5k piece quantities. For more information, please visit: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-qualified

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com