Search
Languages

Bourns Extends Voltage Range of Popular High Power TVS Diode Product Series

RIVERSIDE, Calif., November 19, 2015 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the extension of the voltage range of its popular high power TVS (PTVS) diode PTVS3 product series. The new 15 V bidirectional high current PTVS diodes are designed to meet the protection needs of DC power supplies and power management systems with 12 V batteries. Designated Model PTVS3-015C-TH, the latest high current bidirectional TVS diodes from Bourns offer bidirectional port protection meeting IEC 61000-4-5 8/20 μs current surge requirements. When compared to typical competing MOV technology, the use of Bourns' innovative silicon technology in the Power TVS products provides a lower clamping voltage under surge, greater performance stability and increased reliability.

"Based on customer demands, Bourns added the new lower 15 V PTVS model to our line-up giving exposed and/or harsh environment power supplies the protection they need," said Ben Huang, Product Line Manager at Bourns, Inc. "What makes these new devices ideal is that they exhibit an excellent surge response versus temperature where the maximum surge current at 150 °C exceeds 70 % of their rated value at 25 °C."

Pricing and Availability
As a pricing reference, the Bourns® Model PTVS3-015C-TH is priced at $9.90 each in 50 piece quantities. The new model is available now and is RoHS compliant* and halogen free**.

To learn more about the Bourns® Model PTVS3-015C-TH, please visit the Power TVS Diode product page.

* RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.
** Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com