Search
Languages

Bourns setzt mit der Einführung seiner neuen FLAT® GDT-Produkte den neuen Standard für kompakte Größe und platzsparendes Schaltkreisschutzdesign

RIVERSIDE, Calif., September 29, 2015 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new Gas Discharge Tube (GDT) series using a breakthrough flat package design setting a new standard in volume and space-saving circuit protection design. The 2-electrode Bourns® Model 2017 Series FLAT® GDT uses a breakthrough flat package and horizontal circuitry design to innovatively meet the more sensitive overvoltage protection requirements of high density and space-restricted applications such as telecommunications and industrial communications equipment, surge protective devices and printed circuit board (PCB) assemblies. The new series delivers a 75% savings in volume as compared to standard 8 mm Bourns® GDTs. When vertically mounted, the Model 2017 Series is capable of supporting approximately twice the number of GDTs in the same board space as compared to similar board space using surface mount 8 mm Bourns® GDTs.

In addition to reducing height and overall volume, Bourns' new FLAT® GDT technology is able to maintain the device's robust isolation and current-handling overvoltage protection capabilities. This new compact GDT solution offers superior surge current ratings, low leakage and insertion loss with constant capacitance regardless of voltage. These devices also do not impact signal or system operation due to their voltage limiting capabilities optimized for long-term reliability and performance to satisfy the needs of today's more complex electronics equipment.

"Significantly saving valuable printed circuit board space that helps solve one of the major issues of higher density application design, Bourns® FLAT® GDTs maintain the key features and critical protection benefits of conventional GDT technology. Pioneering the next standard in miniaturizing circuit protection design, Bourns' engineering team employed a unique isolation pathway to ‘squeeze' the GDT in the axial direction resulting in significantly reduced height and volume as compared to similarly-rated conventional GDTs," said Kurt Wattelet, product manager at Bourns, Inc.

The Model 2017 Series is an ITU K.12 Class III GDT device rated at 10 kA on an 8/20 μs waveform. The series features DC breakdown voltages ranging from 90 to 500 V. Maximizing its design flexibility, the FLAT® GDT offers multiple mounting options including bottom-side PCB, and is available in horizontal and vertical surface mount versions as well as a leadless design for cartridge or clamp fit applications.

Pricing and Availability
The Bourns® Model 2017 FLAT® GDT is RoHS compliant* and available now. As a pricing reference, the Bourns® Model 2017 is priced at $ 0.48 each in 1,000 piece quantities. For more information, please see the Bourns® FLAT® Series product page.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com