Search
Languages

Bourns Announces Low Profile, Highly Robust Common Mode Chokes with High Current Capacity for Power Applications

New Common Mode Chokes Deliver Common Mode and Differential Mode in a Single Surface Mount Design Suitable for DC Power Line Applications

RIVERSIDE, Calif., December 9, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced two new low-profile, high current series of compact surface mount common mode chokes. The new SRF1206A and SRF9045A series provide not only common mode but also differential mode filtering in a single choke configuration. These highly robust products offer high current capacity to answer the need for components that meet board space constraints in an increasing number of DC voltage domain applications with voltages up to 80 VDC and currents up to 8 A. This feature makes Bourns' latest common mode chokes excellent solutions for DC-DC converters, switch-mode power supplies, battery management and power line noise suppression in consumer, industrial and other electronics applications.

The SRF1206A and SRF9045A series are AEC-Q200 compliant with operating temperature ranges from -40 to +125 °C, and provide high impedance over a broad frequency range to suppress electromagnetic interference (EMI) either coming into or out of systems. Both series of common mode chokes use separate sector-wound winding configurations, and feature U-shaped terminals clamped to core for superior strength to handle various mechanical stresses. These series also feature a protective plastic shield that protects the part's surface and wires and enables Hi-Pot capability of 500 VAC @ 3 mA, 1 second. In addition to the normal common mode impedance that these components are designed to achieve, this construction also features increased differential mode impedance at a high frequency range.

Bourns® SRF1206A and SRF9045A series are available now, and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com