Search
Languages

Bourns Announces POWrFuse™ High-Power Fuse Series Optimized for High-Voltage EV/HEV Application Accessory Circuit Protection

Bourns® POWrFuse™ Model PF-K series is designed to ISO 8820-8 standards

RIVERSIDE, Calif., August 29, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new POWrFuse™ High-Power Fuse model series. Bourns specifically designed the POWrFuse™ Model PF-K Series to meet ISO 8820-8 standards for the protection of high-voltage accessory circuits in electric vehicles (EVs) and hybrid electric vehicles (HEVs). These circuits are found in a variety of EV/HEV applications including electrical energy storage (ESS), battery disconnect units (BDUs) and battery management systems (BMS).

These new high-voltage EV fuses support operation up to 500 VDC and feature a 20 kA at 500 VDC interrupting rating and an extended temperature range of -55 to +125 °C. Individual models within the PF-K Series have current ratings from 15 to 50 A and are available in bolt and PCB mounting options. In addition, the latest POWrFuse™ EV fuses have been tested to Bourns’ internal automotive quality standards for environmental reliability, transient current cycling and device electrical and fusing characteristics.

The Bourns® POWrFuse™ Model PF-K Series models are available now and are RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/fuses/powrfuse-high-power-fuses#ev

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf